10/5/2021 10:07 AM | |
Joined: 4/28/2015 Last visit: 4/30/2024 Posts: 3345 Rating: (377)
|
Hi, looks like you are using the Industrial OS V2.1.1 and not the Example Image V1.1.1. When using the Service Stick and the menu to install software, npm gets installed when installing node-red. Have you tried to plug the Service Stick and install node-red like explained in this document on page 25. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
10/16/2021 1:49 PM | |
Joined: 3/21/2019 Last visit: 3/22/2024 Posts: 6 Rating: (0) |
Welcome back, I found some time and come back to this topic. I created a new USB Service Stick. After connecting and restarting the iot, I re-installed of the Industrial OS system. Then I reconfigured First Setup according to your instructions. However, I found a difference with the manual. I did not find the Node-RED rule in the Firewall. But after finish the configuration and reboot iot, Node-RED is installed. Unfortunately, I can run but I can't enter the Node-RED system. I use adress: 127.0.0.1:1880 and 192.168.2.150 (I connect through putty at this address). If I connect an SD card with an example image, I can enter the Node-RED system, but I still can't install any additional libraries. There is still a warning for missing modules. Should I use the USB Service Stick also for the system on the SD card (Example Image V1.1.1)? Why on iot system I can use command mel-setup, and on SD card system don't work (with sudo also doesn't work)? I think I'm doing something wrong but I don't know what yet. Best regards! AttachmentScreenshots.pdf (321 Downloads) |
11/9/2021 8:27 AM | |
Joined: 3/21/2019 Last visit: 3/22/2024 Posts: 6 Rating: (0) |
I apologize for the long break. I send my flow in the attachment. Throughout this time, I have not found a solution to the problem. Best regards! Attachmentflows.zip (316 Downloads) |