7/23/2014 9:03 AM | |
Posts: 17 Rating: (0) |
Hi and thx for reply, I attache here the print with the error. Specify that I have a TIAP V12 and I don't find what sp is, suppose that sp1.
Attachmentpic.zip (221 Downloads) |
Last edited by: THUAIA at: 7/23/2014 9:08 AM |
|
7/23/2014 9:19 AM | |
Posts: 17 Rating: (0) |
I also have another version of TIAP V11 SP2 on a other pc and gives the same error |
7/23/2014 9:40 AM | |
Posts: 5225 Rating: (1196) |
...... ,,,,,, Thank you for the image. It is extremely helpful to visualize your problem. I could however not replicate the same results as you have (using TIA11 SP2 Update 5 and TIA13.. I do not have TIA12). I have tried to make spaces between the writing as you have - - no such luck. I do not know why this error will occur. ..unless - - - what is the part number of the PLC? - - - which TIA12 service pack/update? Please review the images attached - see if you can follow the steps. The idea in these are that you do not type out everything.. * you start writting "array"; and the select array from the dropdown list. * next let the system put array of bool * then fill in the needed paramaters. Please see if this helps any. w AttachmentVisual step by step 3.zip (239 Downloads) |
Last edited by: William B. at: 7/23/2014 9:43 AMNOTE: Did read note from THUAIA about trying steps on TIA11 |
|
This contribution was helpful to1 thankful Users |
7/23/2014 9:51 AM | |
Posts: 17 Rating: (0) |
product release is V12.00.00.00_33.25.00.04
Attachmentpic2.zip (217 Downloads) |
Last edited by: THUAIA at: 7/23/2014 10:02 AM |
|
7/23/2014 10:41 AM | |
Posts: 17 Rating: (0) |
Is working. I begin a new project and was no prb. Sorry for headaches and thx for help.
|
This contribution was helpful to1 thankful Users |
Follow us on