2/7/2012 8:36 AM | |
Joined: 9/30/2005 Last visit: 10/1/2024 Posts: 42 Rating: (13) |
Hello dgc, You have to use the special memory card (6ES7954-8LF00-0AA0) Greetings |
2/7/2012 9:54 AM | |
Joined: 8/31/2010 Last visit: 9/30/2024 Posts: 1522 Rating: (228) |
It can't be so, check if the file name you downloaded is 212-1HD30-0XB0_V220.exe |
Like it? Rate it! |
|
2/7/2012 3:14 PM | |
Joined: 8/31/2010 Last visit: 9/30/2024 Posts: 1522 Rating: (228) |
Hello dgc, You need this - 6ES7954-8LE01-0AA0if the extracted files are less than this card size, then it should work. This card will definitely work - 6ES7954-8LF01-0AA0for OS update of S7-1200 to Firmware v2.2 |
Like it? Rate it! |
|
2/7/2012 3:23 PM | |
Joined: 2/6/2012 Last visit: 10/3/2024 Posts: 33 Rating: (1) |
Ok, I will try with that card. Thanks very much for the responses! Best Regards
|
Follow us on