8/4/2014 9:51 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (713) |
Hello, Cpu's with firmware 1.0 can't be updated to V3, i think 2.2 is the highest version. you will find the updates Here, look for the right partnumber and click the link for a short description how to perform a update and the firmware . Regards, Marcjan |
Problem solved? |
|
This contribution was helpful to2 thankful Users |
8/4/2014 11:18 AM | |
Joined: 10/20/2011 Last visit: 3/22/2024 Posts: 102 Rating: (3) |
Dear sir, Thank you for your kind reply.you r correct.Please send me the procedure expect using MMC or web server.
|
8/6/2014 6:09 AM | |
Joined: 10/20/2011 Last visit: 3/22/2024 Posts: 102 Rating: (3) |
Dear sir, Please send any other procedure to upgrade Firmware Without using MMC. |
8/6/2014 7:18 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (713) |
Hello, The only other way to update firmware is through a webserver, that is only possible as from firmware version 3. How do you perform a firmware update for the S7-1200 as from V3.0 in STEP 7 (TIA Portal) by means of the web server? Regards, Marcjan |
Problem solved? |
|
8/6/2014 8:43 AM | |
Joined: 10/20/2011 Last visit: 3/22/2024 Posts: 102 Rating: (3) |
Dear sir, Can able to use 12MB memory card for Firmware upgradation ? |
8/6/2014 8:57 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (713) |
Hello, I don't think so because
What CPU do you have there? Please give us the full partnumber(6ES7 xxxx). Regards, Marcjan |
Problem solved? |
|
8/6/2014 9:13 AM | |
Joined: 10/20/2011 Last visit: 3/22/2024 Posts: 102 Rating: (3) |
Dear sir, CPU - 6ES7 214-1AE30-0XB0 (1214C DC/DC/DC) Version - 1.0
|
8/6/2014 3:01 PM | |
Joined: 7/7/2010 Last visit: 5/17/2024 Posts: 14751 Rating: (2374)
|
Using the right MMC Version 1.0 can be updated to Version 2.2. To get to version 3.0, you need a new PLC - different part #. The latest is version 4.0, and yes, it is also a different part #. |
science guy |
|
8/6/2014 3:21 PM | |
Posts: 5225 Rating: (1187) |
Carefull.. please allow me just fill in the detail that was implied. The jump to 4.0 is huge - hardware and firmware (as was the case with 3.0). You can not get to 4.0 via 3.0. w |
Last edited by: William B. at: 8/6/2014 6:03 PMchange word order to better English sentence structure |
|
8/6/2014 6:01 PM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (713) |
I guess that is wat Huggy means by this, to get FW4.0 you need to buy a CPU with firmware 4.0 But anyway the CPU TS has can't be updated to V3.0 or higher, 2.2 is the max., can only be updated by MMC of atleast 24MB. No other options if the FAQ and manuals are correct. Regards, Marcjan |
Problem solved? |
|
This contribution was helpful to1 thankful Users |
8/11/2014 6:23 AM | |
Joined: 10/20/2011 Last visit: 3/22/2024 Posts: 102 Rating: (3) |
Dear sir, The firmware upgrade(v2.2) file is of 8mb only. Then why we cannont use 12MB card.Any reason behind this. |
Last edited by: Rajesh_s at: 8/12/2014 8:29 AM |
|
8/12/2014 8:31 AM | |
Joined: 10/20/2011 Last visit: 3/22/2024 Posts: 102 Rating: (3) |
Its urgent.Please kindly reply to this issue. |
8/12/2014 9:12 AM | |
Joined: 10/20/2011 Last visit: 3/22/2024 Posts: 102 Rating: (3) |
dear sir, I can have 12MB Memory card with me.Can i use this memory card to update firmware process. |
8/16/2014 4:14 PM | |
Posts: 8 Rating: (0) |
I just wanted to say this has been helpful to me as well thank you. |
8/19/2014 2:39 PM | |
Joined: 10/20/2011 Last visit: 3/22/2024 Posts: 102 Rating: (3) |
Dear all, Successfully done firmware update using the 12 MB memory card. Thanks to all |
This contribution was helpful to1 thankful Users |
1/7/2015 2:47 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4772 Rating: (123) |
|
10/14/2016 9:15 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4772 Rating: (123) |
New question published by fabiogno is split to a separate thread with the subject Can I use Memory Card 12M to update firmware of CPU 1214C?. Best regards |