10/19/2015 2:57 PM | |
Posts: 439 Rating: (109) |
Hello Yeliz, If you have a HMI connection and the HMI tag are related with this connection, then you should take a look at the PLC protection. Did you set a protection access password in the properties of the PLC? If so, then you should enter this password in the properties of the HMI connection. I add a example project to my post. You need to retrieve it with "Project" > "Retrieve" because it is an archived project. If you have more question, do not hesitate. A good way for us to find a solution to your issue would be for you to give us your project. Best regards, Hugo AttachmentTo delete.zip (222 Downloads) |
10/20/2015 9:36 AM | |
Posts: 68 Rating: (0) |
I couldnt attach files as they r too large Which way i can use to send u those files. Do u have gmail? |
Last edited by: yeliz08 at: 10/20/2015 9:39:39 AM |
|
10/20/2015 10:09 AM | |
Posts: 68 Rating: (0) |
I am sending as xps files. If we can find other way to send large size files, i can send original files, as well.
Attachmentprints.rar (239 Downloads) |
10/20/2015 3:36 PM | |
Posts: 68 Rating: (0) |
Ok. I will try to pay attantion. I m very new in programming :( I have another question. When i type a value in I/O field, the value which i type is seen on the screen for 2 seconds but turns into 0 immediately. I have attached short video to show that. Do u have any idea about reason for that? Attachment20151020_164626(1)(1).mpeg4.aac.mpeg4.aac.mpeg4.aac.mpeg4.aac.mpeg4.aac.rar (210 Downloads) |
Last edited by: yeliz08 at: 10/20/2015 4:07:22 PM |
|
Follow us on