6/23/2018 12:12 PM | |
Posts: 2 Rating: (0) |
My SIMOTION D435-2 have a problem. Why? How to do? |
6/25/2018 3:57 AM | |
Posts: 2 Rating: (0) |
Thank you verymuch. Graeme |
Last edited by: armnaja at: 6/25/2018 3:57:47 AM |
|
10/12/2018 9:19 PM | |
Posts: 7 Rating: (0) |
Hello Armnaja, I have the same problem even the fan is running well and the cf card pretty new. Did you solve your problem ? |
10/17/2018 8:20 AM | |
Posts: 7 Rating: (0) |
Hi Christoph i have an Simotion D435 see attached file and an CF Card Simotion D4x5-2 V4.4 HF1. |
10/17/2018 9:01 AM | |
Posts: 7 Rating: (0) |
Hi Christoph , yes, I did see attached file( content.txt) from the card. I also change the simoton module and have the same state. I am working long time with simotion but never had this problem before. I have deleted the user file therefore when we power on simotion put an new user file, but no success AttachmentCONTENT.TXT (218 Downloads) |
10/17/2018 10:31 AM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985)
|
Hello, which MLFB have the Card? do you mea a other Simotion CPU or othe fan module? Regards Christoph |
10/18/2018 10:08 AM | |
Posts: 7 Rating: (0) |
Hi pigroplc, where is the destination file for the image D4xx_D4x5_2_boot1024 to the cf card |
10/18/2018 11:59 AM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985)
|
C:\program files (x86)\siemens\step7\u7umc\images |
10/20/2018 12:43 PM | |
Posts: 7 Rating: (0) |
Hi ChristophD, that is the source file where i take the boot image, now i need the destination file into the cf card. Thanx |
10/22/2018 6:33 AM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985)
|
the destination is the card itself, not a file on the cards. Regards Christoph |
4/1/2019 2:02 PM | |
Posts: 6 Rating: (0) |
Thanks for the interesse to help! Could I create the bootloader at a normal card or just at SIEMENS CARD? In Attachment follow my currently CF! |