5/13/2020 10:18 AM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Hi qwazee, Thank you for answering. Please see the attached screenshots. I want to use the FB in the "new" project with the same functionality as in the "old" project. I already copied the FB from one project to the other and it did NOT tell me that it had created any new DB. I had to change the name from FB100 to FB101 since the new project already had a FB100. As the second screenshot shows there are plenty of static variables used in the FB so I need to copy the corresponding DB also - so how do I identify it and how do I link FB101 to the copied DB (I might have to change the number of the DB also)?
AttachmentEB5 FB101 A.zip (350 Downloads) |
9/15/2022 11:33 AM | |
Joined: 6/17/2016 Last visit: 10/4/2023 Posts: 6 Rating: (0) |
Maybe try, Mouse right Click -> Call Structure |