12/1/2017 12:09 PM | |
Posts: 17 Rating: (0) |
IS THIS |
12/1/2017 12:22 PM | |
Posts: 17 Rating: (0) |
MY MODULE ET200S IS? |
12/1/2017 12:36 PM | |
Posts: 17 Rating: (0) |
I AM STILL NOT ABLE TO CRUSH THE PROFIsafe MODULE |
12/1/2017 12:41 PM | |
Posts: 17 Rating: (0) |
to whatch the rack of the ET200S and the slot Could I see it in properties of the object? |
12/1/2017 12:49 PM | |
Posts: 17 Rating: (0) |
this module can not be plugged in here, only DP slaves can be used in a master system, IT IS THE MESSAGE |
12/1/2017 12:54 PM | |
Joined: 5/12/2006 Last visit: 6/29/2024 Posts: 22290 Rating: (2996)
|
Hi, boah! Drag&Drop it in a slot inside the station! |
12/1/2017 12:58 PM | |
Posts: 17 Rating: (0) |
DO NOT LEAVE ME, THE MESSAGE IS THAT, THIS MODULE CAN BE INSERTED IN THE FRAME 0 TIMES |
Follow us on