3/11/2015 10:34 AM | |
Posts: 5 Rating: (0) |
Dear All, I have Redundant CPU 412-5H configuration system. i have to communicate 3rd party device (DCS). how to configure between my Redundant CPU 412-5H and DCS. Is required any module/software for that configuration. Note: I have interface with my I/O module through PROFINET. Regards, M.Prakash
------------- |
Last edited by: Min_Moderator at: 3/11/2015 11:26:24 AMNew subject after splitting |
|
3/11/2015 8:41 PM | |
Posts: 3093 Rating: (323)
|
Hello Mprakash, Regards, |
3/12/2015 1:01 PM | |
Posts: 5 Rating: (0) |
Dear sir, I am going to use Modbus TCP/IP protocol between my CPU 412-5H & DCS. Best Regards, M.Prakash |
3/12/2015 1:32 PM | |
Joined: 9/27/2006 Last visit: 6/7/2024 Posts: 12260 Rating: (2670) |
Hello Prakash; Have a look at the following FAQ.
and follow the links that point to :
Modbus/TCP
RED V2
Hope this helps, Daniel Chartier |
7/26/2015 11:39 AM | |
Joined: 8/28/2013 Last visit: 12/28/2023 Posts: 1 Rating: (0) |
Is this with integrated PN interface or via CP 443-1 |
7/27/2015 11:17 AM | |
Posts: 3093 Rating: (323)
|
Here you can find an overview of the libraries: https://support.industry.siemens.com/cs/ww/en/view/103709414
Regards, |