5/20/2022 10:32 AM | |
Joined: 5/3/2018 Last visit: 12/5/2023 Posts: 56 Rating: (0) |
Hi All , How do I interconnect these devices in my Tia Portal v16. 1. CPU 1517-3 PN/ DP : 6ES7 517-3AP00-0AB0 2. DP/PA Link with IM 153-2 OD : 6ES7 153-2BA70-0XB0 3. DP/PA Coupler FDC 157-0 : 6ES7 157-0AC85-0XA0 4. Emerson 3051 Press Transmitter ( PA ) : rmt14444.gsd have attached the gsd file. Now i followed this link https://support.industry.siemens.com/cs/us/en/view/26562190 and integrated my Emerson pa transmitter with DP PA Link using gsd file . Using this procedure I am able to integrate but in the link this procedure is telling about connection to non-Step 7 devices using GSD file. The only non - step 7 device here is my Emerson Press transmitter whose GSD file I have combined with the DP/PA link IM module and imported to the hardware catalog. By using this procedure I am able to connect to my PLC and configure dp/pa link and pa transmitter. Now if i import this gsd file of Emerson 3051 Press Transmitter ( PA ) alone i don't know how to configure and interconnect it with DP/PA Coupler FDC 157-0, DP/PA Link with IM 153-2 OD and CPU 1517-3 PN/ DP. I am having confusion setting network speeds of DP/PA Link with CPU (1.5 mbps) and DP/PA link with FDC (45.45 kbps(31.25kbps)) and FDC( all STEP 7 devices) with GSD file of Emerson PA transmitter in Tia Portal V16. Need help in connection between DP/PA Link with IM 153-2 , DP/PA Coupler FDC 157-0 and CPU 1517-3 PN/ DP and GSD file of PA device. If anyone finds step by step configuration document it helps. The only document I get is about "Connection to non-step 7 systems via GSD files" which works fine even with my configuration . What I am looking for is any document about " Connection to Step7 devices via GSD Files". Even the above link talks about how to connect IM 153-2 in the DP/PA link to an external master or a Simatic S5. I am looking for something like how to connect IM 153-2 in the DP/PA link to Simatic S7 1500 CPU. In the attached image I need help with configuration A. Thanks
|
Last edited by: Raghu Kodi at: 05/20/2022 10:33:47Last edited by: Raghu Kodi at: 05/20/2022 10:36:57Last edited by: Jen_Moderator at: 05/20/2022 12:25:07Link optimized. |
|
5/20/2022 10:19 PM | |
Joined: 9/21/2006 Last visit: 5/25/2023 Posts: 247 Rating: (61) |
There is a How do you configure the DP/PA link in the external master or in STEP 7 (TIA Portal)? document that might be helpful. It looks to me like you need to set up your transmitter within the DP/PA link configuration - see figure 7 in the document. |
This contribution was helpful to1 thankful Users |
Follow us on