6/25/2010 9:23 PM | |
Joined: 9/27/2006 Last visit: 4/30/2024 Posts: 12257 Rating: (2666) |
Hello tarek; With all drives that I know you can implement digital or analog controls, so you can start/stop and vary the speed and rotation of your motor through digital and analog outputs. Parameters in the drive and connection terminals will vary depending on the selected drive, so we must have more details to help you more. This is an example of digital and analog speed reference selectiuon for Micromaster (MM4) drives: http://support.automation.siemens.com/WW/view/en/30563620 Hope this helps, Daniel Chartier |
6/26/2010 3:40 PM | |
Joined: 9/27/2006 Last visit: 4/30/2024 Posts: 12257 Rating: (2666) |
Hello tareq; The following manual is for G110 setup and commissioning: http://support.automation.siemens.com/WW/view/en/20976910 Sturdy with carechapter 6 on Commissioning,it discusses such issues as digital and analog controls, fixed setpoints, and parameter, which will be useful when designing your application. Take the time to understand what you want to do, how you want to do it, and use the Search box at the top right of this page to locate other documents that are available on the subject here. Then, when you have precise questions, come back here to get more ideas. Hope this helps, Daniel Chartier |