7/25/2018 6:26 AM | |
Posts: 8 Rating: (0) |
Hi, [snip] One issue I am facing is how to power on the SIM7000e on reboot. I can use node-red to send a pin high to pwr for 2 seconds and it works connecting pin 6 to pwr of Sim7000e. The issue is however that node-red takes a while to load. What would be the easiest way to automatically turn on Sim7000e on boot and start pppd session. I'm thinking it may be easiest to use a Linux GPIO in a script that sets value to 1 and then somehow checks modem is responding and run /usr/bin/pon. Any tips on the best way to monitor connection and restart would be appreciated without using ping. I am thinking that checking something like "ip link show ppp0 | grep -c UP" might work built into a script. Thanks, Antony ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/25/2018 10:57:59 AMNew subject after splitting. Division of questions into separate topics. |
|