8/30/2019 12:39 PM | |
Joined: 12/13/2015 Last visit: 8/23/2023 Posts: 2 Rating: (0) |
Can anybody help me on how to transfer these attached arc files. it will be need either winpcin or sinucom software. these software can be install on windows7 pc or not. I have following versions. and these files should be transfer to sinumeric 810d unit or to hmi. OP270 (6AV6 542-OCC10-0AX0) SINUMERIC 810D Regards jamshaid Amin ------------------------------------------------------------------------------------------ AttachmentNC_Archives.zip (76 Downloads) |
Last edited by: Jen_Moderator at: 08/30/2019 12:45:10New subject after splitting |
|
9/2/2019 12:45 PM | |
Joined: 10/17/2007 Last visit: 5/29/2024 Posts: 3992 Rating: (345)
|
where is the NC.arc file saved? if on the USB stick that will be easy. OP270 have USB port, you can transfer to OP 270, from there you can transfer to 810D. Please refer to your Machine builder manual, as OP270 IS NOT Siemens 810D default HMI WE DON'T KNOW how machine builder designed the transfer menu.
|
If you like my comments please |
|
9/16/2019 1:53 PM | |
Joined: 12/13/2015 Last visit: 8/23/2023 Posts: 2 Rating: (0) |
Thanks. Yes I have this on usb stick. I have attached these files and pictures pls check. and also make me clear either I need any software (like WINCPCIN or SinuARC) to transfer these files to 810D or it will transferred through OP270. If its through OP270 then 1) Pls share the procedure of how can I transfer these files to OP270. 2) Then how to transfer these from OP270 to 810D. OR if I have purcahase WINPC, can I transfer these through My laptop aswell?? AttachmentPICS+NC_FILES.zip (68 Downloads) |