6/14/2011 10:19 PM | |
Posts: 3093 Rating: (323) |
Hi gre_m, but the question was to connect a Microbox and a PAC. Regards, Kaulquappe |
6/17/2011 10:20 AM | |
Posts: 947 Rating: (45) |
Hello Kaulquappe Pac3200 has interface RS485, Profibus and some models ethernet. For Connectby ethernet you can gateway (rs485, profibus) to ethernet. if your model has internal ethernet port? then you can direct connect. PAC3200 use variety TCP - Modbus TCP. You can buy addons from IT4Industry or write own programm. For this need FB for open communication and wizard (That's what I wrote above). Usefull FAQ on customer support http://support.automation.siemens.com/WW/view/en/32048373. No complications in the no. Open communication in WinAC RTX used internal Ports (IF1..IF4) - where in Microbox instaled Profinet card |
Last edited by: gre_m at: 6/17/2011 10:28 AM |
|
Follow us on