11/9/2018 3:34 PM | |
Joined: 10/17/2007 Last visit: 5/4/2024 Posts: 3981 Rating: (340)
|
check attached file for basic test. notice in this writing it missed one indicator--when enabling 64-9, and 63-9 (jumped to DC24V) the green led should be off. for full test you must connect to the machine as there are low control voltage out from flat cable bus which you cannot test by w/o bench (Siemens factory can test, but it to hard for you)
AttachmentChecking procedure of IR-FDD.pdf (323 Downloads) |
Last edited by: nulizhang at: 11/12/2018 7:05:12 PMspelling error correction If you like my comments please |
|
This contribution was helpful to1 thankful Users |