9/28/2016 7:26 AM | |
Posts: 1 Rating: (0) |
sir, I have installed INFORMATION SERVER2014 SP2 SOFTWARE in WINDOWS SERVER 2012 R2 STANDARAD . while i tend to access http//:localhost, "it shows Could not connect to the scheduler service. The service is probably down". how to rectify this problem. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 9/28/2016 4:50:57 PMNew subject after splitting |
|
12/7/2016 3:14 PM | |
Joined: 2/4/2014 Last visit: 3/17/2022 Posts: 28 Rating: (0) |
Dear all, I also faced with same problem. What should be the cause? Thanks in advance. |
2/23/2017 3:39 PM | |
Joined: 4/28/2015 Last visit: 4/19/2024 Posts: 1 Rating: (0) |
Dear all, did you find the solution ? I have the same error message here with Windows Server 2012 R2. Thanks. |
7/13/2017 2:29 PM | |
Posts: 1 Rating: (2) |
Hi, Restart the "Information Server scheduler" services. |
This contribution was helpful to1 thankful Users |
12/8/2020 1:35 PM | |
Joined: 8/1/2012 Last visit: 2/3/2021 Posts: 3 Rating: (0) |
... or check your Information Server license first. Default license is trial, works only 30days, then comes that error. |
12/15/2020 2:50 PM | |
Posts: 5 Rating: (0) |
any change in the computer's date, reset the license usage times, and have to install everything again or place the client's license |
11/2/2022 3:55 AM | |
Joined: 1/11/2012 Last visit: 11/16/2022 Posts: 45 Rating: (3) |
it works |