10/22/2013 7:08 PM | |
Joined: 1/28/2012 Last visit: 7/23/2024 Posts: 519 Rating:
|
If you have Microwin software then check status of Output. . And check wiring also. . |
Regards, |
|
10/22/2013 7:14 PM | |
Posts: 9 Rating:
|
Thanks, Pranav. So, would you say that because the Run light is on, that there is a good chance that the whole part is not "fried" and could be repaired? |
10/22/2013 9:00 PM | |
Posts: 9 Rating:
|
Thanks, Marcjan. Is there some way to reset this sensor so that it will work again? |
10/24/2013 1:51 PM | |
Posts: 9 Rating:
|
Thanks Marcjan, I will try to give it a shot. If you have any recommendations on a good, cheap, small 24vdc battery or other power supply, lemme know. |
10/24/2013 2:11 PM | |
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Hello, First i would not go for battery's, well maybe for a test to see if the system works again with external power. Have a look at the SITOP COMPACT power supplies, i have no idea about the prices, i go for quality. Other brand that might be cheaper is Meanwell. You could have a look at a webshop like Conrad or RS-Online to compare some prices. The powersupply in your CPU was about 300 mA, so i think 1 to 2A must be enough for your system. Regards, Marcjan |
Problem solved? |
|