3/20/2020 10:05 AM | |
Posts: 24 Rating: (0) |
Hello I have a LOGO! 6ED1052-1MD00-0BA8. I learned in this thread I can't work with the advanced web editor but only the simple one. Is this a separate application or is this done by the lwe or by lsc 8.2? Thanks for helping. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/20/2020 11:05:23New subject after splitting |
|
3/20/2020 1:48 PM | |
Joined: 12/18/2014 Last visit: 5/30/2024 Posts: 33130 Rating: (4093)
|
I could, but it wouldn't help ... As written, the extended web server is only available from LOGO! 8.2. Your LOGO! with firmware V1.81.01 is a LOGO! 8.1. The FS is FS04. With this you can update the firmware to a maximum of FS06, which I would definitely do. The firmware version is then V1.81.03. Product information on LOGO! 8 FS:04 and FS:05 The FS4_1 is only a symbolic name for the first inserted FS4-LOGO! in the network view of a network Project. AttachmentVersions of 0BA8.txt (181 Downloads) |
3/20/2020 2:18 PM | |
Joined: 2/22/2008 Last visit: 5/26/2024 Posts: 2698 Rating: (207) |
To answer your actually question, your Logo controller has an internal web page and you need no additional application. You just have to allow the access in the properties of Logosoft. Then use any browser and type in the ip address of the Logo. The shown page is not changeable by the user, but there are some nice options as virtual Logo display or TDE display or variable status. Regards, Scorp |
Last edited by: Scorp at: 03/20/2020 14:19:16 |
|
This contribution was helpful to1 thankful Users |
3/20/2020 3:24 PM | |
Joined: 12/18/2014 Last visit: 5/30/2024 Posts: 33130 Rating: (4093)
|
In attachment a simple program with 4 counters and a message text. If you have enable the web server under access control. To see a message text in the web server you set the check mark in the properties of the message text (see attached screenshot). AttachmentWeb server.zip (179 Downloads) |
3/20/2020 3:26 PM | |
Posts: 24 Rating: (0) |
Do I need the mSD card for the firmware update? Thank you. |
3/20/2020 3:32 PM | |
Joined: 12/18/2014 Last visit: 5/30/2024 Posts: 33130 Rating: (4093)
|
Yes. Everything is in the description on the Website. In this Website is a link to another website: 109750845 |