11/7/2022 9:52 PM | |
Joined: 2/26/2019 Last visit: 11/4/2024 Posts: 57 Rating: (0) |
I am new to LWE and AWS. I've reviewed every post I can find but after about three weeks of trying I'm completely baffled. When I run the LWE APP locally it works fine For this post I've refined my application and LSC program down down to their simplest form, but I can't get my LWE app to connect to my LOGO thing in the cloud in AWS. after I download irt=t to the cloud. After downloading it, LWE sets up an environment.correctly . I've made sure that: 1. I'm running the latest LSC 8.3 SPK 1 and LWE 1.1.1 versions 2. Set my Logo clock before registering it on the cloud 3. Made sure the regions for my AWS thing "TEST_LOGO" and LWE application are the same. 4. Made sure my data cloud transfer settings are set. 5. Tested my Logo online to make sure it's connected to the cloud 6. Set up my LWE IOT of things and tags are correct and referenced in my LWE app. PLease help, I'm sure it's something really simple that I'm missing. My LSC password is LOGO Thank you, Dennis AttachmentTest.zip (743 Downloads) |
11/11/2022 2:16 AM | |
Joined: 12/18/2014 Last visit: 11/7/2024 Posts: 34158 Rating: (4254)
|
I can't say what you doing wrong. I can say only: I've tested your LSC diagram and your LWE project. I load both on my LOGO!. When I try to reach the web server, I become no connection. So I made a new LWE project (Test_2) and this works. Attachmentddingman.zip (966 Downloads) |
Last edited by: ixo65 at: 11/11/2022 02:17:34Attachment |
|
This contribution was helpful to1 thankful Users |
11/11/2022 10:25 PM | |
Joined: 2/26/2019 Last visit: 11/4/2024 Posts: 57 Rating: (0) |
Unfortunately it's a feature they don't support. |
Follow us on