2/22/2016 6:46 PM | |
Joined: 5/30/2014 Last visit: 4/25/2024 Posts: 1 Rating: (0) |
what the minimum SD/MMC is possible use in S7 1200?? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 2/23/2016 12:53:08 PMNew subject after splitting |
|
2/22/2016 7:15 PM | |||||||||
Joined: 3/28/2015 Last visit: 5/10/2024 Posts: 721 Rating: (213) |
Hello, Perhaps the following topic might help:
|
||||||||
Eng.Mohamed Ibrahim |
|||||||||
This contribution was helpful to1 thankful Users |
4/17/2016 9:53 AM | |||||||||||||||||||||||||||||||||||||||||||||||||
Joined: 5/28/2008 Last visit: 5/11/2024 Posts: 4506 Rating: (836) |
Hello, Here's bellow the complete list of all memory cards for CPU S7-1x00
Hope this helps. |
||||||||||||||||||||||||||||||||||||||||||||||||
Ayman Elotaify |
|||||||||||||||||||||||||||||||||||||||||||||||||
This contribution was helpful to3 thankful Users |
4/17/2016 10:15 AM | |
Joined: 5/28/2008 Last visit: 5/11/2024 Posts: 4506 Rating: (836) |
Hello, Normally the usage of MMC in S7-1X00 is to store the program. Please see this old link: Usage of S7-1200 Memory CardA small Car?!!! How much is this small car!! |
Ayman Elotaify |
|
4/17/2016 3:34 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307) |
Hello |
There is no such thing as the last bug in a program |
|
This contribution was helpful to2 thankful Users |
4/19/2016 7:27 PM | |||||||||
Joined: 5/28/2008 Last visit: 5/11/2024 Posts: 4506 Rating: (836) |
Hello EIC Control, The above list is an old list. The complete list of memory cards that can be used for S7-1x00 is provided in my first post here. |
||||||||
Ayman Elotaify |
|||||||||
4/29/2016 2:34 PM |
|
Posts: 198 Rating: (36) |
very very expensive does any one explain what is inside expensive thing?
|
Last edited by: EIC_CONTROL at: 4/29/2016 2:35:29 PM |
|
4/29/2016 3:14 PM | |
Joined: 5/28/2008 Last visit: 5/11/2024 Posts: 4506 Rating: (836) |
Yes it's too expensive. But nobody can tell why it is too expensive. In my opinion, I prefer to make logging on a PC using WinCC TIA is better and cheaper than using these SD cards. |
Ayman Elotaify |
|
This contribution was helpful to1 thankful Users |
4/29/2016 5:43 PM | |
Joined: 7/7/2010 Last visit: 5/10/2024 Posts: 14709 Rating: (2356)
|
What I've gathered is Siemens purchases strict quality control manufactured SD cards with way more capacity than stated on the package. The card has some hidden data with serial number and such so it can be set with know-how protection & licenses. I do not know if the SD / MMC card manager on the PLC or PG/PC monitor the card for errors and reallocate spare storage as required to keep it fully functional, or if it double writes the data for a built-in backup??? But with extra capacity, it could certainly do that.
|
science guy |
|
This contribution was helpful to2 thankful Users |
Follow us on