10/14/2018 6:06 PM | |
Posts: 7 Rating: (2) |
Dear Sir, First of all I am really very very thankful for your quick response. I have no words to show my expressions I am really in great trouble these days Now come towards the problem that I am facing from last 7 days. I am trying to communicate Shinko controller DCL 33A with my PLC. I use pin 4,8 and 11 of CP341 RS422/RS485 and 1(COM), 3 and 4 of Shinko Controller (The manual of controller is also in the attachment, the important points that I used is also highlighted). I also swap the wire many times but it proved not fruitful for me. Before Swap: Pin 4 (CP341) with Pin 3 (Shinko controller) Pin 11 (CP341) with Pin 4 (Shinko Controller) Pin 8 (CP341) with Pin 1 (Shinko Controller) After Swap: Pin 4 (CP341) with Pin 4 (Shinko controller) Pin 11 (CP341) with Pin 3 (Shinko Controller) Pin 8 (CP341) with Pin 1 (Shinko Controller) Note : I also try to use master - salve without GROUND, in short I try to use almost all options regarding WIRING point of view but no results. Also verified the cable multiple times by mean of DMM (Digital Multimeter) One more thing is also very interesting; whenever i follow AFTER SWAP wire connection both TX and RX light blinks but when we power OFF - ON the CPU the CP goes to fault mode and red SF light shows on the CP. So I am sure AFTER SWAP wiring option is not the correct one. Please find the attachments for more details. I am really really very very thankful to you, please guide me. Kind Regards
AttachmentPART1.zip (715 Downloads) |
10/14/2018 6:12 PM | |
Posts: 7 Rating: (2) |
AttachmentPART2.zip (736 Downloads) |
10/14/2018 6:24 PM | |
Posts: 7 Rating: (2) |
AttachmentSlave Information.pdf (810 Downloads) |
Last edited by: projects_mes at: 10/14/2018 6:24:47 PM |
|
10/14/2018 6:26 PM | |
Posts: 7 Rating: (2) |
Dear Sir, I also PM you, Waiting for your kind help Kind Regards
AttachmentShinko DCL 33A Protocol.pdf (744 Downloads) |
Follow us on