1/5/2009 11:01 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello alindsay81, Look a this FAQ: What is the significance of the initial and actual values of a data block? regards |
This contribution was helpful to1 thankful Users |
1/5/2009 1:24 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello alindsay81, I am glad to heard that problem has already solved. regards |
5/15/2009 4:58 PM | |
Joined: 9/23/2005 Last visit: 4/29/2024 Posts: 4325 Rating: (1426) |
Hi, when I sad: "generally, it is not necessary to copy the actual values to initial values, " it was the initial values never goes to the CPU, just the actual values. Normally, programer mount a empyt DB for machine data, for example. In start up it full the values on the VAT." |
Denilson Pegaia |
|
5/15/2009 5:15 PM | |
Joined: 1/4/2008 Last visit: 2/27/2024 Posts: 703 Rating: (96) |
Hello mynamesnotnick, who cares about the initial values? In the FAQ UMENCHO linked to is written that they aren't used by the CPU so only you need are the actual values to save in load memory and/or offline program folder which is such easy! Didn't you mistakenly twisted in mind the initial values with the first time declared actual values in offline? Regards Sydney |
Last edited by: Sydney at: 5/15/2009 5:16 PM |
|
5/15/2009 8:19 PM | |
Joined: 10/23/2005 Last visit: 3/31/2020 Posts: 81 Rating: (9) |
So the whole point is why does Siemens even show an Initial value at all. This just confuses peoplethat are familar with other PLCsoftware. I say just display what the actual value is period. |