11/6/2009 8:43 AM | |
Joined: 11/6/2009 Last visit: 2/21/2024 Posts: 3 Rating: (0) |
Hallo Keyan, If you have a inclined wheel or a inclined wheel and a inclined axis you have to input the right angle in the tool - data Important is you have to input the wheeldataunder zero degree expample Diameter 500 width 80 Z-Position 0 Swivel angle on dressing 30 On the next page geometry-data overflow X 10 overflow Z 10 .... shoulder height 72.36 ... usable wheel width 50.59 The height and the width depends on the angle an will calculated internal by a cycle. For the value of the D-Number please have a look at the documation how it work. Important is also if you have a inclined axis your Reset-Mode for the tranformation should be activ so the the transformation ist activ after reset, because yout have differnt coordinationsystem between transformation and without transformation. Please check MD 20140 = 1 24100 = 1024 24110[0] = 1 24110[1] = 2 24120 [0] = 1 24120 [2] = 2 24700 = your angle of your inclined axis if it is fixed When you register the dresser or workpiece you can have a look in the extend-data of thetool an there you see the calculated value for D1 to D6 for the wheel and D7..D9 for the dressers. Best regrads AttachmentKeyan.zip (87 Downloads) |
Last edited by: Hofmann at: 11/6/2009 9:00 AM |
|
This contribution was helpful to1 thankful Users |
11/11/2009 7:28 AM | |
Posts: 13 Rating: (0) |
Thank you very much, for your valuable replay. but still i am having some doubts in filling parameters for dressing.i attached my problem and my wheel geomentry details. so kindly go through my problems ,and help me. YOURS TRULY, keyan AttachmentWHEEL GEOMETRYDETAILS.zip (83 Downloads) |