8/23/2011 10:05 AM | |
Posts: 267 Rating: (22) |
Hi, your real hardware is the same? Only the CPU 1214C AC/DC/RLY? No signal board? No communication module? |
8/23/2011 3:31 PM | |
Posts: 60 Rating: (6) |
If you go to the hardware configuration screen and go online, what is displayed? Does it identify a specific module as being incorrect? |
8/23/2011 3:45 PM | |
Joined: 5/7/2011 Last visit: 11/4/2023 Posts: 14 Rating: (2) |
Hi I have same problem as @Plazz. I use also MMC card. CPU 1214 DC/DC/RLY. regards
|
8/24/2011 11:01 AM | |
Joined: 5/8/2009 Last visit: 4/18/2024 Posts: 5 Rating: (0) |
Hello I have te same problem, only if i use MMC Card, without difference if i use 2MM or 24 MB card. |
8/24/2011 1:41 PM | |
Posts: 267 Rating: (22) |
Hello, please try the latest firmware V2.1.2: http://support.automation.siemens.com/WW/view/en/41886031/133100 This should solve the problem. |
8/31/2011 9:59 PM | |
Joined: 12/27/2007 Last visit: 8/21/2022 Posts: 12 Rating: (0) |
Hi Freak, i have this problem too using CPU1214 DC/DC/DC with 2 Mb MMC card. i followed your suggestion and downloaded 214-1AE30-0XB0_V212.EXE. I run it and selected directory root of MMC Card. but during the process of unzip is stopped suddenly. and it says there are no enough space on MMC card. Because i use 2 Mb MMC card. in this case, how can i update last Firmware? Regards, Ahmet. |