9/5/2005 2:42 PM | |
Joined: 8/10/2005 Last visit: 4/9/2024 Posts: 1486 Rating: (32)
|
Dear Mr, you don´t have to do an OS-update on OP25 separately. The image will be transfered automatically by downloading the project. An OS update is necessary when the WinCE version that is on the WinCE device (OP/TP170, OP/TP270, MP270, MP370) is incompatible with the WinCE version of the ProTool /Lite /Pro implemented on the configuration computer How to do an OS update (operating system update for WinCE panels) with ProSave V6.0 SP2 please take a look to following link: http://www4.ad.siemens.de/WW/view/en/14293838 Best regards Your Technical Support for Automation & Drives SIEMENS AG |