11/19/2012 6:59 AM | |
Posts: 6 Rating: (0) |
No, since it's not a permanent fault. It only happens when I try to start the drive. I can set parameters as much as i want to. |
11/19/2012 9:38 PM | |
Joined: 3/25/2008 Last visit: 9/27/2024 Posts: 194 Rating: (8) |
One So the defective internal source. Or on the internal fan in the drive. |
9/17/2013 2:57 PM | |
Posts: 2 Rating: (0) |
Hello Christian, I have the same problem. Is your problem alreadysolved and how did you fix it? Thanks, Gino |
Last edited by: Gino de Jonghe at: 9/17/2013 2:57 PM |
|
9/23/2013 7:03 PM | |
Posts: 6 Rating: (0) |
Hi Gino Yes I got it solved. Had to replace all the capacitors, and it has been running ever since. Regards Christian Clavilla Holt |
10/15/2013 8:55 PM | |
Posts: 2 Rating: (0) |
Christian, Thanks. Today I had another one (MM430 7,5 kW) with the same problem. I wil check the capacitors. Thanks for your help. Gino |
Follow us on