8/11/2016 6:34 PM | |
Posts: 68 Rating:
|
Ok what now? |
Last edited by: simatics7300 at: 8/11/2016 6:34:40 PM |
|
8/12/2016 7:28 AM | |
Joined: 5/12/2006 Last visit: 7/10/2024 Posts: 22308 Rating:
|
wrong question! are the adpaters now listed in PG/PC or not? The Add/Remove should not be used. Regards Christoph |
8/12/2016 10:34 AM | |
Posts: 68 Rating:
|
In cmd I see comuniation which tell me that the name "s7epaim6x.exe" is unknow . It is no good. |
8/12/2016 10:43 AM | |
Joined: 5/12/2006 Last visit: 7/10/2024 Posts: 22308 Rating:
|
this is ok because is not named s7epaim64x is it s7epaimp64x! |
This contribution was helpful to
1 thankful Users |
8/12/2016 12:55 PM | |
Posts: 68 Rating:
|
THank you soo much!!! Now I can use PCadpater.auto, but I have problem with TCP/IP interface. Have you an idea? |
8/12/2016 1:37 PM | |
Posts: 68 Rating:
|
PC is connected to the PLC. See a photo. How can I ping the PLC IP from the PC? |
8/16/2016 11:56 AM | |
Posts: 68 Rating:
|
In screen I show ping PLC IP. How can I check if I choose the right adapter ? |
Follow us on