11/17/2017 11:21 PM | |
Posts: 1 Rating:
|
The linked example uses a KTP-700 which is a basic panel not a TP-700 comfort panel. Makes a difference with what you can do with it. |
11/23/2017 5:00 AM | |
Posts: 6 Rating:
|
You can configure the LOGO as a Modbus slave and use anything which can access MODBUS TCP, if you do not have any other Modbus masters on the network... |
11/23/2017 7:54 AM | |
Posts: 2930 Rating:
|
Hi, time has changed also related to LOGO!. New option which may be interesting for you: 1. LOGO! Access Tool: to get data out of LOGO!8 in RUN and store it as CSV. 2. LOGO! Web-Server Both is free of charge. The Web-Server is integrated in any LOGO! 8, the LOGO! Access Tool you can download free of charge from the LOGO! Internet page. In December a new LOGO! 8 is announced with a Web-server allowes used defined web-pages. Hope this helps |
Follow us on