11/13/2012 8:55 AM | |
Posts: 6 Rating: (1) |
Dear Wüstenräuber, I have restarted the PLCs by tricking them into downloading the hardware again, so that the installation won´t stop. I have observed that whenever I make a petition to read/write I get directly an error in the module and no busy or done is ever activated, they are always 0. I attach the chart. It is the one giving me the problem. AttachmentUOperate.pdf (258 Downloads) |
11/13/2012 10:07 AM | |
Posts: 3093 Rating: (322)
|
Hello Thanasis, which Modbus block and version do you use? Regards, Kaulquappe |
11/13/2012 10:35 AM | |
Posts: 6 Rating: (1) |
Hello! It's Open Modbus/TCP Redundant Communication. MB_REDCL Version 2.0. FB909 by default. Cheers, Thanasis |
11/13/2012 11:01 AM | |
Posts: 3093 Rating: (322)
|
Hello Thanasis, there is a hotfix available regarding the communication lock up after restart. You can order it at it4.industry@siemens.com by telling them the license number of the Modbus library. Regards, Kaulquappe |