3/16/2009 10:35 AM | |
Posts: 92 Rating: (7) |
dear Mr.Razi, please check the following on your side, 1. please find the settings on your comuter should be as in attachment_1. 2. ensure that the plc connection in ON from CNC. Attachmentattach_1.pdf (862 Downloads) |
3/17/2009 9:36 PM | |
Posts: 433 Rating: (48) |
Hi is_razi, did you contact your local siemens sales partner regarding your question? Tomcat |
3/17/2009 10:28 PM | |
Joined: 3/13/2009 Last visit: 6/4/2024 Posts: 131 Rating: (1) |
thanks to your gidances i have solved the problem. |
1/6/2011 2:54 AM | |
Posts: 2964 Rating: (481)
|
Hello..... Could you check this link it will be useful...... /tf/WW/en/Posts/52129 yes it possible to establish in both the interface... you need to go to set PG/PC interface there you need to make the selection.....check the above link Regards, Ekalavya |
1/3/2013 6:35 PM | |
Posts: 288 Rating: (4) |
I am waiting for your help.
|
1/6/2013 5:10 PM | |
Joined: 11/26/2006 Last visit: 3/13/2024 Posts: 36 Rating: (5) |
Same problem today with V3.1 Programming Tool PLC802,and fresh installation of WIN7.I have installed TIA portal V11 too.And after one day trying and mistakes, the solution is- Open regedit,and merge/802.reg/ This file adds PLC802(PPI) to thelistof installed protocols.And then,same procedure with / progtool.reg / ,which is added protocol to Progtool. I hope this help. AttachmentDesktop.zip (459 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on