10/24/2008 9:34 AM | |
Posts: 13 Rating: (0) |
As far as i have been able to figure this out, this isn't possible. Too bad though |
11/12/2008 2:53 PM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating: (102)
|
Hello at all I thing, Z-tech´s problem can be solved in two ways. Both ways are no easy. Fist way: (PSC 7 like - multi-instance Faceplate) *You can create one (normal)Faceplate for one robot (from the Example) - http://support.automation.siemens.com/WW/view/de/24449702/0/en - http://support.automation.siemens.com/WW/view/en/23130773 *Youuse "TagPrefix" foryourtags form the first Faceplate (multi-instance) - http://support.automation.siemens.com/WW/view/en/23689276 - http://support.automation.siemens.com/WW/view/en/22789387 Second way: *You define an Information-Area andControl-Area - In the Information-Area are displayed the informations of theselectedrobot(Example) - In the Control-Area are Buttons (60), witch call a skript with there name as input-value - The skript put the Informations in the Information Area. So you create the button one and copy it how much you need. - for alarms and warnigs, you create textfieds or something else and change thetext and the colorof it. These textfields were also filled by an skript, witch look at the alarm-tags by change. You can handl it so, thatyou create one textfield and copy it how much you need. Thats a to comprehensive projekt / application, to discribe here.I thing you should create your own Faceplate, its the better way. I hope i understand you rigth and i could help you. Good luck cumulus |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|