7/8/2010 2:47 PM | |
Posts: 739 Rating: (55)
|
to store a data-set in the AOP, you have to delete a language. But be aware that this deleted language can´t be restored! see FAQ-cluster: http://support.automation.siemens.com/WW/view/de/26435762 |
12/4/2014 9:34 PM | |
Posts: 33 Rating: (7) |
I just had this happen to a customer, deleted 2 languages, uploaded program, when it was finished it went blank. any ideas??? It is connected to a MM440 |
6/16/2016 9:26 AM | |
Joined: 4/28/2009 Last visit: 6/7/2024 Posts: 336 Rating: (41) |
Hello, I tried to solve this problem with blank screen (4 dead AOPs...). I receive recommendation to do "power on" (remove and return back to drive) on AOP after language deleting. AOP during startup reorganize its memory and than should not be a problem with upread/download parameter set. With regards Martin ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 6/16/2016 9:55:10 AMNew subject after splitting |
|
11/21/2017 2:43 PM | |
Joined: 6/19/2017 Last visit: 6/7/2024 Posts: 8136 Rating: (165) |
New question published by jaafer is split to a separate thread with the subject Is there any way to recover the AOP firmware without replacing the whole AOP? . Best regards |
My Forum is the place to personalize your profile, |
|