10/5/2018 2:00 PM | |
Joined: 4/28/2015 Last visit: 4/24/2025 Posts: 3345 Rating:
|
Hi community, we have finally released the Profinet Driver for the IOT2000. For the Profnet Package you will get a Realtime Image for the IOT2000 and the PN Driver itself. The complete documentation about the API is included as well as a IOT2000 specific Getting Started. With this package you can use the IOT2000 as Profinet Controller. For now you will have to send a private message in the forum including your email address, then I can send you all the required things. In the next step you can donwload these things from Siemens Industry Online Support like you know from the IOT2000 Example Image and the SDK for Eclipse. Have fun and best regards! ------------------------- UPDATE ------------------------- You can now download the Realtime Image and PN Driver on the Siemens Industry Online Support Pages! https://support.industry.siemens.com/cs/ww/de/view/109761191 |
Last edited by: bergmanu at: 10/5/2018 2:01:07 PMLast edited by: bergmanu at: 2/12/2019 4:16:00 PMSIOS Link available Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to
5 thankful Users |
10/8/2018 1:45 PM | |
Joined: 12/12/2016 Last visit: 7/25/2025 Posts: 640 Rating:
|
Hello, The functionality is equivalent to the previously known PROFINET Driver for controllers. You can also find some info about V2.1 here. Kind regards! |
1/9/2019 4:08 AM | |
Posts: 1 Rating:
|
i need,thank you [snip] |
Last edited by: Jen_Moderator at: 1/9/2019 7:46:47 AMRemoved E-Mail address. |
|
2/12/2019 4:16 PM | |
Joined: 4/28/2015 Last visit: 4/24/2025 Posts: 3345 Rating:
|
------------------------- UPDATE ------------------------- You can now download the Realtime Image and PN Driver on the Siemens Industry Online Support Pages! https://support.industry.siemens.com/cs/ww/de/view/109761191 |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to
2 thankful Users |
8/22/2019 10:06 AM | |
Posts: 2 Rating:
|
Hi, bergmanu, I have followed the PNDriver_QuickStartIOT2040.pdf (2,7 MB), and finnished the steps in chapter 2.2.1, but when I execute command "lsmod" , there is no "PnDevDrv 32" in the output. Here is my system version: root@iot2000:~# cat /proc/version Linux version 4.4.154-cip28-rt20 (oe-user@oe-host) (gcc version 7.3.0 (GCC) ) #1 PREEMPT RT Wed Nov 7 09:19:23 UTC 2018 Could you help me with it? Thank you! |
11/4/2019 11:18 AM | |
Joined: 12/12/2016 Last visit: 7/25/2025 Posts: 640 Rating:
|
Hello, The Profinet Driver is not Open Source, so we cannot provide the sources. We updated the PNDriver to work with V2.4.0, it should be available on here (PN_Driver_IOT2000.zip) in the next days, with a new hash: 25dc9785aa580fac417a01ae168ec85f27a348e44c83858784d07b8697b5d6f3 If you need it urgently, please send me a pm with your Email and I can provide it to you. Kind regards! |
12/29/2019 11:30 PM | |
Joined: 2/16/2017 Last visit: 3/15/2024 Posts: 5 Rating:
|
FYI: the device driver sources I received (well, the GPL parts of it) can be found here: pndev-driver at sourcehut I fixed a minor issue and added a build manifest (as a buildroot package) so the sources can be tested in that regard. They still don't support kernels newer than 4.4, as far as I see (4.9 and above didn't work, IIRC). Porting work to current kernels shouldn't be hard but I don't have the capacities for it right now. Here's an example pndev driver build |
Follow us on