10/9/2014 7:40 AM | |
Posts: 102 Rating: (2) |
Dear Fellows, I am using Simatic manager step 7 V 5.5 and WINCC V 7.0. I have integrated my WINCC project in step 7 as shown in attached image 1, and the total size of program has become almost 65.4MB. The size of my code is shown in image 2. My memory card is 512KB. Now when i click on PLC > Save to memory card. It gives error as shown in image which states that not enough memory. Will i have to purchase a 65MB card now? or is there any other solution?
AttachmentNew folder (2).zip (145 Downloads) |
10/9/2014 8:14 AM | |
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181) |
For sure the card should be big enough. |
10/9/2014 9:16 AM | |
Posts: 784 Rating: (52) |
Hello, Have you try "Compress memory"? Best regards.....
|
Follow us on