8/31/2016 9:32 AM | |
Posts: 291 Rating: (1) |
Hello Christoph The screenshots are attached,please see them.The lib LMCIpr will use the lib LMCBasic internal. when i compile the LMCBasic for the device D425v4.1 , it is ok, but when i compile the LMCIpr for the D425V4.1 it says: it is not available for the D425 , does the LMCIpr have more requirements? (FOR examole version ....)?? Thank you very much!
Attachmenterror and setting picture.doc (91 Downloads) |
9/1/2016 3:52 AM | |
Posts: 291 Rating: (1) |
Hello ChristopD I use the Device D425 V4.1, in my project ,i want to use 4 libs, LDPV1 ,LMCBasic ,LMIpr, LPrsH, The LDPV1 and LMCBasic is ok when i compiled them, but the LMIpr and LPrsH have many errors , please see the attachment. Thank you ! AttachmentNeu Microsoft Word-Dokument (2).doc (78 Downloads) |
Follow us on