1/27/2012 6:01 PM | |
Joined: 6/4/2008 Last visit: 4/23/2024 Posts: 1481 Rating: (322)
|
Hi, First things first, if you are a beginner, I would strongly recommend that you access the MM4's by the more traditional methods of sending data (upto 8 words) from/to a PLC to dedicated areas withing the MM4 (i.e. r2050[0] to r2050[7]) using standard telegrams. From here, they can then be read and connected anywhere in the inverter. The LADDR of the drive remains the same. HOWEVER, if you do want to directly control parameters such as P1082 (which is a numerical entry), then this can be achieved, please refer to thisFAQ, but be warned, this is quite advanced. Regards, Graeme EDIT: To be specific, please refer to the section header -
|
Last edited by: Graeme at: 1/28/2012 6:10 PM |
|