5/3/2013 9:58 AM | |
Posts: 61 Rating: (0) |
Hello Saravana kumar thank you for reply and help. I'm new in this so what you write is Sci-Fi for me I need some time to convert it to LAD language, so I can understand what you write, then I will come back if I have question and I know that i will |
5/3/2013 1:18 PM | |
Posts: 61 Rating: (0) |
First of all thank you for your time and help. I try to write your program but as I expected lot off unknown in Network 5, but I use ADD_DI as you told me and it is working like I want to. Is this correct ?? Best regards, Goran AttachmentOB1.pdf (155 Downloads) |
5/3/2013 3:07 PM | |
Posts: 197 Rating: (3) |
Dear Saravana kumar,
QUIT:NOP 0 |
5/4/2013 5:31 AM | |
Joined: 2/6/2009 Last visit: 8/19/2024 Posts: 939 Rating: (118) |
Hi, Thank you, There are so many ways to write a logic. Your logic also works. See the below for writing the same logic in different way, A( AI0.0 LL#1 NOP 0 |
_______________________________________________________________ |
|
5/4/2013 5:41 AM | |
Joined: 2/6/2009 Last visit: 8/19/2024 Posts: 939 Rating: (118) |
Please add a one second pulse bits in the place highlighted in the pdf as shown in my previous thread.
AttachmentOB1.pdf (184 Downloads) |
_______________________________________________________________ |
|
This contribution was helpful to1 thankful Users |
5/5/2013 3:41 PM | |
Posts: 197 Rating: (3) |
Dear Saravana kumar,
Thanks for the reply. What I meant is your 1st post had counting on MD100 and I suspected it would go on counting disregarding the CPUCLOCK PULSEor the MOTOR FEEDBACK( and I tested it on simulator, MD100 actually goes on counting). Regards |
Follow us on