8/17/2015 6:08 PM | |
Posts: 45 Rating: (0) |
Sure, I will do that and send you the dropbox link. Thanks |
8/17/2015 6:12 PM | |
Posts: 45 Rating: (0) |
AttachmentReference - 2.rar (212 Downloads) |
8/18/2015 9:10 AM | |
Joined: 5/12/2006 Last visit: 6/4/2024 Posts: 22254 Rating: (2986)
|
Hello,
the D435 you use can't be updated to Version V4.4 . https://support.industry.siemens.com/cs/de/en/view/31045047
Regards Christoph |
Last edited by: ChristophD at: 8/18/2015 10:34:13 AM |
|
8/19/2015 9:53 AM | |
Posts: 45 Rating: (0) |
Hello, When i m doing fw update then the error come and still i am not able to update fw.Can you please give me the steps of fw update of "D435 Control Unit; Firmware V4.2 - PN V2.2 with SINAMICS S120 V2.6.2" 6AU1 435 -0AA00-0AA1 / V4.2
|
8/19/2015 10:24 AM | |
Joined: 5/12/2006 Last visit: 6/4/2024 Posts: 22254 Rating: (2986)
|
Hi,
ok if you use the device tool to create the update data you need the FWSP installed. The first link is the FW only, normaly extract the downloaded FW Zip File to the Root of a empty SIMOTION CF Card and put it in the CPU , the new FW is now loading at bootup from the CF Card. Note that you must also change the Version of the CPU in the project to V4.3 ! To do that open HWConfig and select the D435 V4.3 in thew HW Catalog and Drag&Drop it on the Rack of the D435 Station. If you don't update the CPU Version in the project then the device Tool can create the data for V4.3 and you can't work with the project if FW V4.3 isz on the CPU. I think is better you check if the Proxy init is working in you chase with Version of CPU V4.3. Regards Christoph |
Last edited by: ChristophD at: 8/19/2015 10:28:16 AM |
|
8/19/2015 11:01 AM | |
Posts: 45 Rating: (0) |
Sure i will try , that offline work of device proxy creation. |
8/19/2015 11:11 AM | |
Posts: 45 Rating: (0) |
|
8/19/2015 11:17 AM | |
Posts: 45 Rating: (0) |
|