2/1/2022 3:29 PM | |
Joined: 1/9/2020 Last visit: 7/23/2023 Posts: 21 Rating:
|
Have it up and running now, cant seem to get the network output from client logo to slave logo to work. Have the logos in master and slave mode. In simulation the network output works from LWE, but the signal wont go to the slave logo. Same subnet. Attatching my project Attachment2 logos Verkstan.zip (193 Downloads) |
2/1/2022 3:45 PM | |
Joined: 12/18/2014 Last visit: 8/6/2024 Posts: 33498 Rating:
|
You must allow the S7 access in both LOGO!s. File > Properties > Offline settings > General |
2/2/2022 8:27 AM | |
Joined: 1/9/2020 Last visit: 7/23/2023 Posts: 21 Rating:
|
Still no luck, all the flags in simulation works from LWE, but the Q1 on second logo still not active. Then the inputs I1 and I4 are momentary break, works fine in regular simulation, but when I do the online test and activate from LWE the inputs are not red(active) how come? Attachment2 logos Verkstan V2.zip (211 Downloads) |
2/2/2022 9:54 AM | |
Joined: 1/9/2020 Last visit: 7/23/2023 Posts: 21 Rating:
|
Here is the LWE project. Attachment2logos verkstan.zip (199 Downloads) |
2/2/2022 10:41 AM | |
Joined: 12/18/2014 Last visit: 8/6/2024 Posts: 33498 Rating:
|
Because I have only one LOGO! 8.3, I must change the slave LOGO! to a LOGO! 8.2. Then I chnaged the IP addresses and so on to my addresses. After all this done, I upload the LWE project and the LOGO! programs. And It works. See attached video. AttachmentTest LWE.zip (193 Downloads) |
2/2/2022 3:22 PM | |
Joined: 12/18/2014 Last visit: 8/6/2024 Posts: 33498 Rating:
|
You have to transfer the variable from LOGO! 1 to LOGO! 2. |
2/2/2022 3:32 PM | |
Joined: 1/9/2020 Last visit: 7/23/2023 Posts: 21 Rating:
|
Hm, how do I do that in example? |
2/2/2022 3:46 PM | |
Joined: 12/18/2014 Last visit: 8/6/2024 Posts: 33498 Rating:
|
See attachment ...
AttachmentTest.zip (192 Downloads) |
Follow us on