6/5/2011 2:40 PM | |
Joined: 10/7/2005 Last visit: 8/6/2024 Posts: 3016 Rating:
|
Well spotted dear MatthiasV, that was a test to see if all of this hasn't lead to a brain meltdown |
Last edited by: fritz at: 6/5/2011 3:06 PMgot stung by the end quote bug again .... Cheers |
|
6/6/2011 10:52 AM | |
Joined: 10/7/2005 Last visit: 8/6/2024 Posts: 3016 Rating:
|
you are not doing anything wrong dear MatthiasV. I cut the header of the source file and there's also some "surplus" text in it which was caused when I encapsulated the text in the "Code" brackets. There's two ways to make it workthough 1.) Retype the logic OR 2.) Use the attached source file AttachmentFC10.zip (212 Downloads) |
Cheers |
|
This contribution was helpful to
1 thankful Users |
6/6/2011 6:13 PM | |
Posts: 30 Rating:
|
Thanks that worked (y) Kind regards, Matthias V
|
This contribution was helpful to
1 thankful Users |
4/28/2012 7:20 PM | |
Joined: 4/20/2007 Last visit: 5/27/2024 Posts: 724 Rating:
|
I didn't get that.. Could you explain a little bit more extensive? |
Follow us on