6/29/2022 3:31 PM | |
Joined: 10/11/2006 Last visit: 8/9/2022 Posts: 5272 Rating:
|
Hello noyacbr, |
With best regards, |
|
This contribution was helpful to
1 thankful Users |
6/29/2022 8:28 PM | |
Joined: 12/6/2016 Last visit: 6/30/2022 Posts: 63 Rating:
|
hi friend, Yes you are right, we have several types of cu. This is CU240E-2DP with DI4, DI5 for SAFETY FUNCTIONS. I've been reading about your link and i confused.. i've severa pdf about this. 1. after release the sto the drive is ready SAFETY ready after release sto its ready 2. i need a f-di for ack, then this cu not right because have only two f-di (used for the channels of relay) SAFETY ack with f-DI When you say "start the drive again" you say P840? AttachmentDesktop.zip (1 Downloads) |
Last edited by: Jen_Moderator at: 06/30/2022 09:45:49Links removed and files added as an attachment. |
|
6/30/2022 5:59 AM | |
Joined: 4/23/2010 Last visit: 8/9/2022 Posts: 7672 Rating:
|
Yes. |
6/30/2022 6:54 AM | |
Joined: 6/19/2017 Last visit: 8/9/2022 Posts: 5941 Rating:
|
Hi noyacbr, please attach your files as an attachment and don't use ibb as a filesharing hoster. I can't open and check it, because the website is blocked. If you want to attach more than one file, you can create a zip file to attach more than one file. Best regards, |
My Forum is the place to personalize your profile, |
|
This contribution was helpful to
1 thankful Users |
6/30/2022 8:41 AM | |
Joined: 12/6/2016 Last visit: 6/30/2022 Posts: 63 Rating:
|
Sorry AttachmentDesktop.zip (3 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on