5/16/2007 1:09 PM | |
Posts: 75 Rating: (0) |
What for the service ССEClient necessary? What functions this servicecarries out? |
5/16/2007 1:33 PM | |
Posts: 1084 Rating: (72)
|
Hi, If I'm not mistaken it is used for the Communication Configurator and is used for network connections on the client. with regards, Ikkezelf |
5/16/2007 1:48 PM | |
Posts: 75 Rating: (0) |
But if this service is disable in Windows, may be or not WinCC works propely but once a month WinCC PDL runtime hangs? |
5/16/2007 1:59 PM | |
Posts: 3149 Rating: (171)
|
Hi |
5/17/2007 8:17 AM | |
Posts: 75 Rating: (0) |
We casually have found out that the service CCEClientisdisabled. About once a month WinCC6SP4HF2 hanging (alarm logging runtime working, tag logging runtime working) but graphics runtime don't work. AttachmentDiagnose_OS1.zip (168 Downloads) |
5/17/2007 2:04 PM | |
Posts: 1275 Rating: (123)
|
Hi, Just a curiosity - the files on you .zip were last changed on February 27th, which is nearly 3 months ago... is this when the problem happened, are these logs old, or is your computer's date wrong? 255,05.02.2007,13:02:34:796,1012204,4,,DK5-1NR-1,RedundancyAgent,Internal error! Can not copy DK5-1NR-1_DK5#1NR_ALG_200702051005_200702051011 255,27.02.2007,01:08:12:546,0,4,,DK5-1NR-1,ArchiveManager,Failed to switch archive(Type:1):(null) ! That's all I found. Apparently you've had problems with the redundancy agent. Here's a thread for you to look at. Make sure that ALL your log files are attached always, and attach the new files. Best regards, Danielle |
Follow us on