11/24/2010 5:54 PM | |
Posts: 11 Rating: (0) |
No any error on cpu D410, i use only shift measuring instruction after enable function. thanks jacek |
6/7/2011 1:24 PM | |
Posts: 344 Rating: (50)
|
Are you running the MCC chart in the background on in the motion task? The easiest implementation is to run the function in the motion task. Make sure that the task starts up on power up. Attached is the example motion task program and a screen capture of its execution trace. If you want to run the MCC chart in the background, there are other considerations that must be taken into account: the background task cannot be stopped until the function execution is complete. The function must be called multiple times until it reports complete status. AttachmentShift.zip (106 Downloads) |