8/2/2012 4:52 PM | |
Posts: 1 Rating: (0) |
hello everybody I have a question about the alarm of simotion. (sorry i dont speek English very well) this is for a simotion D410 i want basic alarm for the drive, the motor, etc. i dont want the specific default. just watching "there is a problem with ......" Saisissez du texte, l'adresse d'un site Web ou importez un document à traduire. traduction automatique de Google Alpha I'm looking for a basic alarm to prevent the operator of a default. but the operator does not need detail. is there a solution existing in the system bit or alarmtechnology ? tanks for help |
Last edited by: Romain at: 8/3/2012 11:52 AMLast edited by: Romain at: 8/3/2012 11:50 AMLast edited by: Romain at: 8/2/2012 5:15 PMLast edited by: Romain at: 8/2/2012 5:14 PM |
|