3/13/2018 9:07 AM | |
Joined: 7/30/2012 Last visit: 5/12/2024 Posts: 335 Rating: (12) |
Hi, i've attached the simotion diagnostics image. My i-device communication address in simotion starts from 100 to a total 67 bytes Attachmenterror.docx (360 Downloads) |
3/13/2018 9:11 AM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2986)
|
Hello, ok i wait until you can provide the requested informations.
Christoph |
3/13/2018 9:18 AM | |
Joined: 7/30/2012 Last visit: 5/12/2024 Posts: 335 Rating: (12) |
I've attached the requested information in the format of a word file with this post. I-device communication between et200sp and simotion d425 where et200sp is the controller and simotion is the slave send and receive address in simotion is i100 and q100 for 67 bytes Attachmenterror.docx (274 Downloads) |
3/13/2018 9:38 AM | |
Joined: 7/30/2012 Last visit: 5/12/2024 Posts: 335 Rating: (12) |
ok here it is then. AttachmentDevice Diagnostics.txt (240 Downloads) |
3/13/2018 10:25 AM | |
Joined: 7/30/2012 Last visit: 5/12/2024 Posts: 335 Rating: (12) |
Axis_01_OP_ModeControl - Network 11 has global variable only. This program works perfectly if i set the i-device communication address starting from 0. Ive attached the screenshot of the network along with the diagnostic details of the PLC. One more thing, communication exists between et200sp and simotion AttachmentERROR.docx (253 Downloads) |