4/26/2018 10:59 AM | |
Posts: 15 Rating: (0) |
Hi. Is it possibe to use a MP277 10" with the 425-2? We cent compile and get them to comunicate. Of course its in a hurry. :) |
4/26/2018 11:19 AM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985) |
Hello, which SW do you use? Christoph |
4/26/2018 12:38 PM | |
Posts: 15 Rating: (0) |
We use the TIA 14 Yes, compilation error. |
4/26/2018 12:56 PM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985)
|
Hi, and which compile error or is this a big secret? |
4/26/2018 1:20 PM | |
Posts: 15 Rating: (0) |
I will start the compile again so i can take a snap of the error. |
4/26/2018 1:25 PM | |
Posts: 15 Rating: (0) |
Here it is. |
4/26/2018 1:28 PM | |
Posts: 15 Rating: (0) |
|
4/26/2018 2:00 PM | |
Posts: 15 Rating: (0) |
Do you mean in the HW config? Or the sw in the HMI? We tested 12 in the HW config with the same result. |
4/26/2018 2:02 PM | |
Posts: 15 Rating: (0) |
We get this warning.. |
4/26/2018 2:07 PM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985)
|
this warning is ok because one port from the comfort panel is not available on the MP277 and will be removed. |
4/26/2018 2:10 PM | |
Posts: 15 Rating: (0) |
Do we need to upgrade the hmi to 12, or TIA14 will solve this? We lost the Connection to the HMI when we tried this. |
4/26/2018 2:13 PM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985)
|
the hmi HW? the FW should be downloaded with TIA, if not you can upgrade the HMI Panel with PRoSave. |
4/26/2018 2:24 PM | |
Posts: 15 Rating: (0) |
Get this errorcode every time... |
4/26/2018 2:28 PM | |
Posts: 15 Rating: (0) |
|
4/26/2018 2:28 PM | |
Posts: 15 Rating: (0) |
|
4/26/2018 2:29 PM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985)
|
is the Panel in transfermode? Are you direkt connect from you PC to the Panel? |
4/26/2018 2:43 PM | |
Posts: 15 Rating: (0) |
yes. Direkt connected... |
4/26/2018 2:48 PM | |
Posts: 15 Rating: (0) |
In the old Project in Wincc it worked fine. But after migration, the problem accured. Losing conection when trying to load. Works a while and then error. |
4/27/2018 8:20 AM | |
Posts: 15 Rating: (0) |
Is it possible that the problem is that the HMI we use are 6AV6643-0ED01-2AX0? The new MP277 is 2AX2 |
4/27/2018 1:58 PM | |
Posts: 15 Rating: (0) |
No? Not got any more ideas? |
Follow us on