1/9/2013 1:05 PM | |
Posts: 1530 Rating: (59)
|
Hello ToreK, really a strange behaviour. Nevertheless I would suggest to check necessary rights of windows (again). Maybe somehow a knot came in from this side. For sure you can also contact Siemens Technical Support. Please let me and other forum members know about your solution. Best regards Bizur |
6/1/2014 9:14 PM | |
Joined: 11/29/2011 Last visit: 5/20/2024 Posts: 1358 Rating: (231) |
Hi, I experienced the same issue with PCS7 V8.0 SP2. After the project transfered over to the OS stuck and come back with an error. All looks OK see the attachments. I wonder what am I missing here. Advice appreciated. Cheers
AttachmentOS_UserRight.zip (403 Downloads) |
- What you read here, please check with manuals and your requirements. |
|
6/1/2014 10:36 PM | |
Joined: 10/3/2010 Last visit: 5/24/2024 Posts: 1552 Rating: (188) |
Hey MicroMan, I checked your screenshots in the attached zip. Did you check Simatic Shell in Windows Explorer? open Windows Explorer, rightclick on Simatic Shell and choose update. You should see both PC names. Also check that Simtic Shell is pointing to the correct network card. Do you have the same users with the same password and same rights logged on ES and OS? |
Last edited by: SteBo at: 6/1/2014 10:42 PMLast edited by: SteBo at: 6/1/2014 10:37 PMadded instructions B r g d s , |
|
6/2/2014 9:18 AM | |
Joined: 10/3/2010 Last visit: 5/24/2024 Posts: 1552 Rating: (188) |
hey ToreK, glad it's solved & thanks for letting us know. It's always nice to see someone coming back to make clear that an issue is solved. |
B r g d s , |
|
This contribution was helpful to1 thankful Users |
6/2/2014 11:55 AM | |
Joined: 11/29/2011 Last visit: 5/20/2024 Posts: 1358 Rating: (231) |
Hi, Things I tried this morning. Checked the user rights on ES and OS. Used SimaticRught.Exe on the OS project folder. Reinstalled SQL server on OS server. Nothing so far. There is something I noticed. The user groups on the ES looks a bit different. See the attachements. Maybe that because the ES installation. Is that a problem that the ES is running on Win7 ultimate and the OS is running on Windows Server 2008 r2? Thank you for your help. AttachmentES_OS_UserGroup.ZIP (266 Downloads) |
- What you read here, please check with manuals and your requirements. |
|
This contribution was helpful to1 thankful Users |