8/18/2012 9:20 PM | |
Joined: 10/31/2011 Last visit: 4/29/2024 Posts: 400 Rating: (5) |
Dear sir, i have install wincc7 on windows 7 but there is no station configuration fditor. regards
|
8/25/2012 4:13 PM | |
Joined: 10/31/2011 Last visit: 4/29/2024 Posts: 400 Rating: (5) |
i m asking about station configurator editor which use xdb file. Sorry for spelling mistake...
|
1/19/2013 11:55 AM | |
Joined: 11/7/2011 Last visit: 1/27/2023 Posts: 96 Rating: (0) |
IN MY CASE ALSO THE SAME THING HAPPENED. |
6/20/2013 9:15 AM | |
Posts: 319 Rating: (9) |
While Installing WinCC, you must select Simatic Net option. Station Configuration editor will be displayed only when Simatic Net Software is installed. I have uploaded a image so that you can get a clear idea.
AttachmentOPC.zip (1345 Downloads) |
This contribution was helpful to3 thankful Users |
6/25/2013 6:14 AM | |
Joined: 1/28/2009 Last visit: 6/27/2023 Posts: 25 Rating: (1) |
Hi all, Thanks for your previous answer. Simatic Net is installed now but now I am having a problem with the Station Configurator in this new PC Client station (Windows 7 Pro + SP1) The problem: - I am trying to setup the configuration of the Station to be able to download the project configuration from Simatic Manager - In the "Add Component" window of the Station Configurator when I open the "Type" dropbox the only options that I have are "Application" and "OPC Server" whereas when I setup the other PC clients which have been running on site for more than a year, I had all the usual options including "WinCC Client Application". I already compare installed software versions and everything matches between the running PC clients and the new PC that I am trying to setup now. I tried to reinstall all over again WinCC v7.0 + SP3 and Simatic Net PC Software v8.1 + SP1 (including windows) and I am still having the same problem. I have attached the exported file of the Installed Software for the new PC and a screen capture showing the Station Configurator issue. Do you have any idea why this could be happening?? I look forward to hearing from you soon. Attachment130625 - Windows 7 Client PC.zip (740 Downloads) |
6/25/2013 1:58 PM | |
Posts: 319 Rating: (9) |
Dear CesarL, Have you selected WinCC OPC Server option while installing WinCC Software ? Check the attachment , it will give you a clear picture. With regards, nand gate.
AttachmentWinCC.zip (682 Downloads) |
1/9/2015 3:31 PM | |
Joined: 2/6/2009 Last visit: 4/26/2024 Posts: 46 Rating: (23) |
Hello, Today, I had the same issue with WinCC V70 SP3 and Simatic Net V8.1 SP1 installed on PC running Windows Server 2008 R2 Standard SP1 x64 edition. In Station Configurator of Simatic Net was no WinCC application offered in add component menu, even these software's are correctly installed. In compatibility lists, all software packages are represented as compatible. I tried to import station with xdb file, but got message "The component is not installed". Several reinstallations with different order were generating the same problem, no matter what. After applying a service request I got the solution that fixes this issue. See attached files. Hope this will help to others. Best regards, VladD AttachmentWorkaround_WinCC-Application_EN.pdf (1366 Downloads) |
This contribution was helpful to10 thankful Users |
1/9/2015 3:32 PM | |
Joined: 2/6/2009 Last visit: 4/26/2024 Posts: 46 Rating: (23) |
And second file. P.S. I cannot attach 2 files in one post? Why? Best regards, VladD
AttachmentFix.zip (1059 Downloads) |
Last edited by: VladD at: 1/9/2015 3:32 PM |
|
This contribution was helpful to10 thankful Users |
2/11/2015 12:30 PM | |
Joined: 9/29/2005 Last visit: 5/3/2024 Posts: 5 Rating: (1) |
Works also on Win7 SP1 x64 Simatic NET V8.1.2 |
5/31/2015 2:24 PM | |
Joined: 4/14/2015 Last visit: 1/25/2024 Posts: 8 Rating: (0) |
thanks my problem is solved |
Last edited by: vagish1111 at: 5/31/2015 2:24:27 PM |
|
7/1/2015 3:49 PM | |
Joined: 9/19/2013 Last visit: 4/19/2024 Posts: 21 Rating: (0) |
Thank you Sir. |
4/15/2016 12:15 PM |
|
Joined: 7/13/2009 Last visit: 4/15/2024 Posts: 137 Rating: (5) |
Thanks for the post. I too faced the same problem and solved. |
Thanks and Regards |
|
5/25/2017 6:45 PM | |
Posts: 1 Rating: (0) |
Thank you for the your answer ! |
9/12/2017 4:32 PM | |
Joined: 4/29/2014 Last visit: 1/30/2024 Posts: 2 Rating: (0) |
Thank you! It was a great solution. |
9/28/2018 6:23 PM | |
Joined: 4/15/2017 Last visit: 5/6/2024 Posts: 3 Rating: (0) |
Thank you so much VladD... your solution solved my problem too.( WinCC V7.3SE & Simatic NET V12). |
Follow us on