4/26/2018 9:07 AM | |
Posts: 10 Rating:
|
do you mean this? |
4/26/2018 9:19 AM | |
Joined: 5/12/2006 Last visit: 8/5/2024 Posts: 22334 Rating:
|
he mean the ordernumber of the IM Module., |
4/26/2018 3:51 PM | |
Posts: 10 Rating:
|
Oh, i see... Thanks, it's 6ES7 151-1BA02-0AB0 :D |
4/28/2018 2:53 AM | |
Posts: 10 Rating:
|
Hi, I have installed STEP 7 Safety Advanced V14 SP1, because mine was SP1 and it said can't install the previous one, (not SP1) but my migration is still have a problem, here my uploaded migration xml in mediafire. Migration Log AttachmentMigration log.zip (144 Downloads) |
Last edited by: Jen_Moderator at: 4/30/2018 10:16:53 AMDeleted link and added file as an attachment. |
|
5/2/2018 10:37 AM | |
Posts: 10 Rating:
|
I opened the project on Simatic Manager, and then [right click] on bausteine, and select "Check Block Consistency", after that, I clik on the second icon "Compile All", and here the result. I uploaded 3 screenshots, which shows errors from TIA, and then showing the DB13,14, also the I/O access error, and the other is showing the FC90 error on the last row of the compile log. I have right click on each DB which needs recompile, but after I compile it one by one, there is no different. I mean, nothing change, and still shows needed to recompile. AttachmentScreenshots.zip (146 Downloads) |
5/11/2018 6:15 AM | |
Posts: 10 Rating:
|
Hello, I have re-configuring the project, I have compile it, and there's no problem. I have installed the "Migration Tool for Tia Portal sp1", and during the installation, I have checked all the software on the setup. Can you help me, which migration option that i missed? I mean, I have no Idea which setup that i missed the checkbox when installing the program. Is it on the Step 7 v14 installation, S7-PLCSIM, WinCC v14, or else? AttachmentMigration log.zip (120 Downloads) |
Follow us on