4/26/2016 11:20 AM | |
Joined: 8/5/2010 Last visit: 7/30/2024 Posts: 17 Rating: (1) |
Dear Ayman, I'm pretty sure that he has used TIA V11, regards,
Francesco |
4/27/2016 2:37 PM | |
Joined: 5/28/2008 Last visit: 8/5/2024 Posts: 4515 Rating: (838) |
Hello, Then the Panel is working and may be the TIA project is corrupted. You can ask the supplier to send you another project or even "Pack&Go" file to download directly to the MP. May be the problem happen when you tried to edit something in V12 and the main project created in V11. "Pack&Go" is a good solution if you don't want to open the project and make edits in it. The programmer can generate Pack&go file using WinCC flexible or WinCC TIA. How do you transfer a WinCC flexible configuration without configuration software to an operator panel (Pack&Go)? |
Ayman Elotaify |
|
Follow us on